|
The PSM 400 is also setting standards in terms of convenient operation. The latest feature is a swivel arm, which is used for flexibly positioning monitor, mouse and keyboard. assen.
|
|
 |
01-20-2012 -
State-of-the-art technology and ease of use don’t necessarily go hand-in-hand. For the first time, the semi-automatic laser welding machine of the PSM 400 series from SCHUNK Lasertechnik makes both possible. With this machine, small and large components can be precisely machined. Moreover, its ergonomic design prevents fatigue when using for extended periods of time. The latest feature is a new telescopic swivel arm, equipped with monitor, mouse and keyboard, which can be quickly and comfortably adjusted to the individual working position. All the entries can be done in a comfortable seating position. The telecopic swivel arm completes the ergonomic concept of the PSM 400. As in the past, the operator still has convenient access to all machining-, programming-, and control functions, no matter how big the components are. The mobile operation panel with the sensitive joystick can therefore be freely positioned. Moreover, a high-quality swiveling binocular with a swiveling range between 10° and 50° allows for relaxed, high-precision work. An electrically height-adjustable machine table, which can be swivelled to both sides, and an adjustable swivel-mounted laser welding head ensure for maximum flexibility in the working area. And proving that no details were left out, even the ergonomical designed seat can be optimally adjusted to the size and working position of the operator.
|