|
|
News - Clamping Technology - 2013
|
| |
05-06-2013
Universal high-performance lathe chucks
The ROTA NCD wedge bar power chuck from SCHUNK is extremely versatile. It is used for clamping small diameters as quickly and precisely as large ones. Instead of exchanging lathe chucks and collet chucks, which can be tedious, just the top jaws of the ROTA NCD have to be exchanged against special collet jaws. This minimizes set-up times and allows a considerably higher output.
more...
04-18-2013
Greater efficiency with integrated vibration damping
Manufactures who produce precision turned parts in large quantities have to consider several factors. Tolerances and surface qualities have to be precisely maintained, set-up times, downtimes, and tool wear have to be reduced. The TENDOturn hydraulic expansion toolholders from SCHUNK make everything feasible. The set-up process of the latest toolholder generation of the competence leader in clamping technology and gripping systems has been further simplified.
more...
02-26-2013
Extremely flat pneumatic Quick-Change Pallet Module
With a height of 20 mm, the Quick-Change Pallet Module VERO-S NSE mini from SCHUNK is extremely flat. This provides ideal conditions for retrofitting existing machines, making full use of the engine room, and allows direct clamping of small workpieces. The patented drive concept consists of a fast stroke and a clamping stroke, and ensures that the compact module of the innovative family-owned company has a highly compact performance.
more...
01-21-2013
Versatile manual lathe chuck
The manual ROTA-S plus lathe chuck from SCHUNK is a true classic in the field of lathe chuck technology. With version 2.0, the competence leader for clamping technology and gripping systems extends the application possibilities of this lathe chuck. An optimized wedge bar drive system and an improved lubricant system ensure consistently high clamping forces from the new lathe chuck.
more...
01-17-2013
Direct clamping with a membrane
SCHUNK, the competence leader for clamping technology and gripping systems enlarges its program for high-performance direct clamping: the innovative family-owned company has developed the SPM plus 138 fixture membrane made of aluminum, where workpieces of various clamping geometries are clamped from all sides with a pull-down effect.
more...
01-10-2013
Low-cost introduction into the square pole technology
By means of comprehensive standardization, SCHUNK, the competence leader for clamping technology and gripping systems succeeded in providing a very economic introduction of the square pole technology to the average consumer. The investment costs for square pole plates of the MAGNOS Performance Line are 40% lower than conventional, multi-purpose modifiable MAGNOS square pole plates.
more...
|
 |
 |
 |
|
News - Clamping Technology - 2013
News - Clamping Technology - Archive 2012
News - Clamping Technology - Archive 2011
News - Clamping Technology - Archive 2010
News - Clamping Technology - Archive 2009
News - Clamping Technology - Archive 2008
News - Clamping Technology - Archive 2007
News - Clamping Technology - Archive 2006
News - Clamping Technology - Archive 2005
News - Clamping Technology - Archive 2004
News - Clamping Technology - Archive 2003
|