|
|
 |
|
|
Press Release - Gripping Systems - Archive 2007
|
| |
|
11-26-2007
Expansion of series PEH 30/50
SCHUNK has expanded its servo-electric 2-finger parallel gripper of the PEH series to include sizes 30 and 50. This once again significantly expands the application spectrum for this universal long-stroke gripper, because with a maximum stroke of 100 millimeters per finger for the PEH 50, these grippers are now suitable for a large parts spectrum, extending from small components to large workpieces. The robust guides are designed for precise handling even at high loads and they easily withstand high payloads. The gripping force can be adapted to the broad application spectrum – for the PEH 50 as high as 1400 Newtons, with maximum finger lengths of up to 250 millimeters.
more...
|
|
|
11-26-2007
New servo-electric controller from SCHUNK
SCHUNK has developed a new controller, the MCS, which will control all servo-electric automation modules in the future. These modules include the EGN, EZN, PEH, PG and EVG electric gripper series, in addition to the PR, PW, PSM, PDU and SRU-MD rotary modules, as well as the modules of the PRL series.
more...
|
|
|
11-26-2007
Electric gripper with longer stroke: The EGN 80 and 160 from SCHUNK
SCHUNK has expanded its EGN series of electric 2-finger parallel grippers to include the sizes 80 and 160, which have a stroke per finger of 8 and 16 millimeters, respectively. This upward and downward expansion of the series now makes it possible to use the exact size of gripper for each task – with exactly the right specifications, but without over-investing.
more...
|
|
|
10-16-2007
SLH 35 assembly element:
Small assembly profile for the modular system
SCHUNK, the clamping and gripping technology specialist based in Lauffen, Germany, has added a new size to its SLH assembly elements for the GEMOTEC modular system, and now also offers elements for pipe columns with a diameter of 35 millimeters. The new assembly system includes components such as single or double mounting bases and plinths, for example, which are used for supporting the hollow columns and are connected to one another by means of cross connectors and assembly plates. The ground and chrome-plated single or double columns allow simple, precise clamping and fastening of the bases and cross connectors. In this way, a variety of assembly versions can be configured using just a few standard elements. Machined locating surfaces and integrated assembly and locating bores guarantee that elements will be fitted with perfect angular precision.
more...
|
|
|
10-16-2007
MMS-P proximity switch
Two in one: Programmable sensor
With the MMS-P, SCHUNK, the clamping and gripping specialist based in Lauffen, Germany, has added a brand new proximity switch with two programmable switching points to its product range. Now, a single sensor is capable of detecting both the “open” and “closed” states. That means fewer sensors, fewer cables, fewer adjustments – and lower costs!
more...
|
|
|
10-16-2007
MFT material finishing tool: Driven tools for robots
Increasingly, robots are no longer being used just for handling and feeding, but for machining tasks such as drilling, milling, grinding or polishing. With the MFT material finishing tool, SCHUNK, the clamping and gripping specialist based in Lauffen, Germany, now offers an air-driven, slow-running tool with a high torque, which is specially designed for the robot-assisted surface machining of metals and plastics.
more...
|
|
|
09-25-2007
SCHUNK Cooperation with Vision & Control
SCHUNK, the leading technological specialist for gripping technology and automation in Lauffen/ Neckar, Germany is entering a strategic partnership with Vision & Control, the specialist for industrial image processing in Suhl. SCHUNK is expanding its product portfolio to develop its leading position in the field of mechatronic automation. Vision & Control is applying its know-how in a technological sector with outstanding prospects for the future, developing new sales opportunities and at the same time gaining a strong partner for global sales.
more...
|
|
|
09-24-2007
RM 08 / 10 mini rotary modules
They are becoming tinier and tinier, and thereby opening up a world of new possibilities in the miniaturization of production and assembly. With its new RM 08 and RM 10 rotary modules, SCHUNK, the clamping and gripping specialist based in Lauffen, Germany, has further expanded its range of GEMOTEC rotary modules at the miniature end of the scale, and now introduces onto the market two rotary units that are among the smallest specimens of their kind.
more...
|
|
|
09-24-2007
ASP drop blocks for vertical axes
In handling systems, sudden energy losses can lead to considerable damage - not just because grippers can no longer hold their workpieces when the pressure drops, but also because vertically mounted linear modules suddenly lose their grip and commence a rapid journey downwards together with their freight, endangering products, equipment and personnel. Thankfully, SCHUNK, the clamping and gripping specialist based in Lauffen, Germany, provides an effective remedy with its modular ASP drop blocks, which prevent vertically mounted linear modules from falling if there is a loss of pressure. They prevent uncontrolled movements in the event of leakages or emergency stops, thereby increasing the safety of the system as a whole.
more...
|
|
|
09-24-2007
OPS anti-collision and overload protection unit: Improved overload protection
SCHUNK, the clamping and gripping specialist based in Lauffen, Germany, has completely redesigned its OPS anti-collision and overload protection unit, whilst also adding sizes 63 and 125 to the range. There has been a whole range of improvements on the old system, one major result of which has been the complete modification of the monitoring system for recording and indicating collisions.
more...
|
|
|
09-24-2007
Quick-change system with integrated valves
The SWS-I-011 integrated quick-change system from SCHUNK, the clamping and gripping specialist based in Lauffen, Germany, incorporates six rapid-reacting
3/2-way screw-in valves, which replace an entire valve terminal. Instead of a bundle of cables and leads, only one single cable is required for the compressed air supply and one for the power supply - grippers and other tools are actuated by the integrated valves and no longer need separate hoses. The two remaining supply cables can easily be routed inside the arm of Scara robots, and even through center bores only twelve millimeters in diameter.
more...
|
|
|
09-24-2007
MWS miniature changing system: A tiny changer
The MWS miniature changing system with an outer diameter of 20 and 30 millimeters from SCHUNK, the clamping and gripping specialist based in Lauffen, Germany, is an exceptionally flat, compact tool changing system for small robots. The MWS was designed for tasks in the field of micro system technology and handling the smallest of components, and meets the requirements of DIN 32565 Level 4. It picks up both tools and handling devices, and enables not just rapid manual changing, but also the automated replacement of tools when used with the appropriate changer rack.
more...
|
|
|
09-24-2007
SRU rotary actuator: Now in sizes 8 to 14
SCHUNK, the clamping and gripping technology specialist based in Lauffen, Germany, has added sizes 8 to 14 to its range of pneumatic SRU rotary actuators. With its finer size gradations, this series now offers exactly the right sizes for the production and assembly of small components.
more...
|
|
|
09-24-2007
EVG 2-Finger Parallel Gripper: A sensitive touch with adjustable length
With the development of its completely new EVG series, SCHUNK, the specialist in toolholding, workholding and gripping technology located in Lauffen, Germany, offers an electrically powered, adjustable length 2-Finger Parallel Gripper, with a stroke that can be largely adapted to individual requirements. The EVG series is available in two standard sizes, with strokes of 40 or 100 mm. Thanks to the mechanical design, the stroke can be easily adjusted to specific customer requirements.
more...
|
|
|
09-24-2007
JGZ: New centric gripper from SCHUNK
SCHUNK, the clamping and gripping technology specialist based in Lauffen, Germany, has restructured its range of pneumatic grippers and divided it into three segments. In future, the middle segment will be formed by the "SCHUNK Compact" gripper class, which will provide all the essential functions. This class can also be extended with plenty of accessories and offers an excellent price-performance ratio.
more...
|
|
|
09-24-2007
JGP: New parallel gripper from SCHUNK
SCHUNK, the clamping and gripping technology specialist based in Lauffen, Germany, has restructured its range of pneumatic grippers and divided it into three segments. In future, the middle segment will be formed by the "SCHUNK Compact" gripper class, which will provide all the essential functions. This class can also be extended with plenty of accessories and offers an excellent price-performance ratio.
more...
|
|
|
09-24-2007
Formed by laser
SCHUNK, the specialist in toolholding, workholding and gripping technology located in Lauffen, Germany, now offers polyamide gripper fingers and adapter plates. They are manufactured in a laser forming process by LMD, the technology partner of SCHUNK. Components, manufactured by this process can feature very complex geometries, which cannot be produced by metal cutting technologies - or only in an enormous time-consuming and cost-intensive way. For example, complex air feed-throughs can be routed through one-piece workpieces in all three dimensions, without having to set bore holes from the outside.
more...
|
|
|
09-24-2007
SCHUNK now with Machine Vision Sensor
The SRV from SCHUNK is a vision sensor for industrial image processing, which is able to complete numerous image processing tasks without any further peripheral equipment.
more...
|
|
|
09-17-2007
MAGNOS MAU Magnetic Gripper:
Auto-magic gripping!
SCHUNK, the specialist in toolholding, workholding and gripping technology located in Lauffen, Germany, now offers an innovative way of handling ferromagnetic workpieces. Until now, magnetic clamping technology was mainly used in stationary workholding systems. The MAGNOS MAU magnetic gripper now offers a completely new perspective. Adapted to fit on a robot arm, it ensures a secure hold at very limited space requirements at a low weight. With the MAGNOS magnetic gripper, handling ferromagnetic workpieces is extremely easy. In the process, the electro-permanent magnets can be activated in seconds. Even in case of power outage, the magnet grippers ensure an absolutely secure hold since electricity is only needed to activate and deactivate the magnets.
more...
|
|
|
01-19-2007
No more loose wiring harnesses!
When a robot has to perform rotary movements, SCHUNK’s DVS rotary distributor is the ideal solution for supplying tools, gripper modules or linear units with air, fluid or electrical signals.
more...
|
|
|
01-19-2007
Everything revolves around the customer
The PRL servo-electric rotary actuator from SCHUNK amtec robotics is freely configurable, thereby allowing flexible robotics solutions to be created to suit individual customer requirements. The PRL enables the creation of reconfigurable, modular robot structures, the individual PRL modules can be assembled with connecting parts with complete freedom and flexibility to produce an individual lightweight arm. Four sizes of modules with different drive torques are available, which can be combined as desired. The PRL is designed as a quill drive, and allows cables and hoses to be routed in a protected manner inside the arm to the front link. In this way, the cables remain invisible and there are no interfering contours.
more...
|
|
|
01-18-2007
For safe production
Robots and handling systems stubbornly follow their programmed course, and if something gets in their way, it can rapidly become very expensive. SCHUNK’s new OPS collision and overload protection provides immediate protection from down-times and high costs. It forms the perfect interface between the gripper and the robot arm, and offers reliable, controlled collision and overload protection with manual reset.
more...
|
|
|
01-15-2007
Optimized to perfection
SCHUNK has completely revised the electric miniature rotary actuators of the MRD series, improving their performance and, above all, making them more user-friendly. The rotary modules are equipped with powerful torque motors, which achieve high torques of up to 3.6 Newton meters even at low speeds, and ensure maximum positioning accuracy of 0.001° at an acceleration of up to 45.000 rad/s.
more...
|
|
|
Press Release - Gripping Systems - 2013
Press Release - Gripping Systems - Archive 2012
Press Release - Gripping Systems - Archive 2011
Press Release - Gripping Systems - Archive 2010
Press Release - Gripping Systems - Archive 2009
Press Release - Gripping Systems - Archive 2008
Press Release - Gripping Systems - Archive 2007
Press Release - Gripping Systems - Archive 2006
Press Release - Gripping Systems - Archive 2005
Press Release - Gripping Systems - Archive 2004
Press Release - Gripping Systems - Archive 2003
|
|
|
|