|
Insiders compare the state of robotics today with the 1970s, when no one really knew what a computer could be used for. Thirty years had passed since Konrad Zuse built his Z3 in 1941. The actual development step was in fact just around the corner. Before the computer was able to begin its triumphal advance, the individual components first had to be optimized, the interplay between the components had to be improved through standards and, above all, affordable components had to be developed. The parallels with service robotics are unmistakable. In the absence of common standards, many developers repeatedly started from scratch and developed their own robotics world, resulting in systems that were incompatible with other solutions. Components were too expensive, and the technology was still immature.
As service robotics solutions are usually used for mobile applications, robot components have to be lightweight, compact and frugal in their energy consumption. It is now becoming apparent that development in this field is accelerating greatly. Among the reasons for this are the greater availability of affordable servo technology, the steady improvement in batteries for mobile applications, the falling costs of processing power and sensors as well as the further development of powerful mechatronic rotary and gripper modules.
As one of the market leaders in the field of gripping systems, SCHUNK GmbH & Co. KG, based in Lauffen/Neckar in Germany, has expanded and enhanced its expertise in this field in good time. The gripping system and robotics specialists at SCHUNK use a system of mechatronic modules, ranging from the servo-electric rotary actuator to the complete lightweight arm and the gripper or even the anthropomorphic hand. This system has proven its worth in practice and is constantly being developed.
|
A study by SCHUNK in collaboration with the University of Linz has shown that humanoid robots that can walk or even climb stairs can be constructed using mechatronic modules.
|