|
|
 |
| |
|
|
| |
 |
|
|
|
|
2007 SCHUNK Synergy
|
SCHUNK Synergy
|
|
|
Toolholding/workholding technology and automation – two core competencies from one source. Live at EMO 2007 SCHUNK presented a machine equipped completely with SCHUNK products - from the spindle to the robotics. SCHUNK Synergy is your added value for efficient production – your competitive advantage!
|
|
|
Start signal for expansion of automation plant
The rapid growth at SCHUNK continues. In Brackenheim-Hausen, a production hall with an area of 5,000 sq. meters with annexed offices is being built directly next to the plant of the automation division. The official ground-breaking ceremony took place on August 3, 2007. Starting in June 2008, about 70 employees will produce customized functional assemblies for automation solutions in the new building.
Product Information
SCHUNK cooperation with Vision & Control
SCHUNK is entering a strategic cooperation with Vision & Control, the industrial machine vision specialist from Suhl. This means that SCHUNK is expanding its product portfolio in order to develop its leading position in the field of mechatronic automation. The competencies of the two technological leaders perfectly complement each other, because machine vision is becoming increasingly important especially in the robot and automation sectors.
Product Information
TENDO-ES hydraulic expansion chuck
|
|
|
The extremely short hydraulic expansion chuck for powerful volume cutting. Maximum holding power and more space in the machine room.
Product Information
|
|
|
SCHUNK SLIM LOCK quick-change system
|
|
|
The worldwide novelty in mould making. The base form concept for hot runner moulds significantly reduces costs and materials.
Product Information
|
|
|
SCHUNK UNILOCK NSA-SF quick-change pallet system
|
|
|
The compact and multi-talented system for automated production. For a perfect connection to the machine table – extremely versatile and variable.
Product Information
|
|
|
ROTA NCS 3- and 6-jaw power chuck
|
|
|
High-precision and low-maintenance. Benefits: axial run-out < 0.01 mm, maximum clamping force, completely sealed.
Product Information
|
|
|
Launch of SRV and new product division MACHINE VISION
|
|
|
With the launch of machine vision SCHUNK is expanding its automation technology products. The new compact SRV all-in-one camera sensor is the flexible solution for a wide variety of sensor tasks in automated production processes. All components are of high quality and are perfectly configured for optimum system performance. And the software for the integrated object and position monitoring is a guarantee for 100% controlled production.
Product Information
|
|
|
New gripper segment – launch of the SCHUNK COMPACT class
|
|
|
Transparency through differentiation. SCHUNK has restructured its line of pneumatic grippers by dividing it into three segments. The middle segment forms the "SCHUNK Compact" gripper class, which provides all essential functions and can be supplemented with many accessories and therefore offers an outstanding price-benefit ratio. Two new grippers mark the start of this new middle class: the JGP parallel gripper and the JGZ centric gripper.
Product Information
|
|
|
Launch of quick-change system SWS-I
|
|
|
The new quick-change system creates maximum flexibility. Six integrated 3/2-way clamp-in valves eliminate not only entire valve terminals, but also the installation of bundled cables and wires. Grippers and other tools can be controlled easily and with very little commissioning effort via the integrated valves – making single hose connections a thing of the past.
Product Information
|
|
|
|
|
|
|