|
|
 |
| |
|
|
| |
 |
|
|
|
|
2011 Future begins today
|
SCHUNK breaks all records
With its superior modular programs, and a richness of ground-breaking innovations, SCHUNK has proven itself to users all over the world. A unique increase in sales across every product range confirms the leading role in the field of clamping technology and gripping systems.
BLUE SIGMA - In total more efficient
|
|
|
SCHUNK celebrates the premiere of more than 40 benchmark products at the EMO show, which allow time, cost and energy saving. The world-wide leading trade show of the machine tool industry becomes the perfect stage for prooving SCHUNK’s competence in leadership and credibly as a world player.
|
|
|
Germany’s best machining mechanics comes from SCHUNK
|
|
|
At an efficiency contest of the federal association "Metal" in Essen, the freshly qualified machining mechanics, Holger Roth leaves its apprenticeship behind and receives the first prize. Therefore he achieves a nationwide top position among the graduates of this training.
|
|
|
Service robotics becomes an economic factor
|
|
|
The 4th.SCHUNK Expert Days on Service Robotics are completely booked before the event took place. At this leading symposium on applied service robotics, numerous practical examples clarify that service robots are increasingly leaving the status of university-based research, and are frequently used by industrial enterprises for specific applications.
News: Industry discovers potentials of service robotics
|
|
|
Superior Lightweight Arm
|
|
|
The LWA 4 Powerball Lightweight Arm is a milestone in the field of service robotics. At a dead weight of 12 kg, it can handle payloads up to 6 kg at an excellent repeat accuracy of 0.06 mm dynamically. These are ideal preconditions for stationary and mobile applications in human environments, and also for industrial handling applications.
LWA 4.6
|
|
|
Standardized Line and Room Gantries
|
|
|
|
|
|
|
New edition of the ROTA-S plus best seller
|
|
|
With the version 2.0, SCHUNK continues the story of success of the highly efficient ROTA-S plus manual lathe chuck. An optimized wedge bar drive and an improved lubrication system ensure enormous clamping forces of the new chuck generation. High torques and cutting speeds allow the use of efficient cutting edge materials, and shorten the production time.
ROTA-S plus
|
|
|
Highly efficient workpiece clamping
|
|
|
The module program for highly efficient workpiece clamping is consistently being enlarged: VERO-S NSE mini, the pneumatic quick-change pallet systemVERO-S offers a very flat design with only 20 mm installation height. It permits retrofitting of existing machines and even small workpieces can be directly clamped. For automated loading, the light and powerful VERO-S NSR robot coupling and the VERO-S NSA plus palettizing module are setting standards. SCHUNK particularly developed the VERO-S NSL turn clamping station for a speedy workpiece change on milling-turning centers.
VERO-S
|
|
|
|
|
|
|