|
|
Applications
Field-proven applications
Here is a small selection of individual solutions for individual industries.
|
A rotary gripping module should be used for simultaneous loading and unloading of a grinding machine with crankshafts in one step.
The conceived functional module is attached to a movable portal. In order to ensure the necessary work safety, collision and overload protection is integrated. If there is a collision, an emergency stop signal is output. Two swivel units are combined with each other. The first one swivels in the x-y plane by 180°, the other turns the workpiece by 30° in the x-z plane. Two dust-tight 2-finger parallel grippers are fastened to the swivel unit via an adapter plate. Both the swivel units as well as the grippers have Viton seals and are operated with an air purge (0.5 bar) to protect them from penetrating coolant. In addition, the grippers each have two torque sensors (supports) and have a workpiece presence check using compressed air.
- Maintenance-friendly cable connectors
- Complete functional module for use in contaminated surroundings.
Crankshafts
Crankshaft
Back to overview, to the search results
|
|

|
|